How Robotics Supports Quality and Growth in Medical Device Manufacturing

"Thanks to the precision and repeatability of our robots, Stäubli completely fulfills the requirements necessary to support the world of medical devices. Our global network of OEMs and system integrators covers all of the specific applications of the industry’s manufacturing processes."

 

Sebastien Lagarde | Global Market Leader Pharma & Medical at Stäubli Robotics 

The spectrum of products within the medical device industry is very large. But from low-value bandages or tongue depressors to CT scanners, all products have one thing in common: Quality is highly regulated with strict standards.

Continuous innovation in this industry, complemented by the connected and wearable device trend, has led to growth in production. When devices need to be personalized for each patient, the complexity of industrial processes reaches its highest, adding traceability to the manufacturing facility’s top criteria.

Robotics accounts for all these requirements when automating repetitive tasks, improving quality by reducing human error, adding transparency and real-time data on produced batches, and bringing flexibility to the manufacturing process for personalized devices.

The high repeatability and precision of our robots reduce variants in the final product while meeting the demands of production growth. Despite general environmental trends, the number of single-use products continues to rise, amplifying the need for scalability at a time when Western countries face a lack of qualified operators.

Factors like these make robotization mandatory. The initial investment can be significant, but the return on investment is predictable, especially regarding high-value medical devices.

While mobile robotics is now ready to be implemented in factories, artificial intelligence, machine learning, and predictive maintenance are expected to reach the next level. Innovation will continue to fuel the industry, both in terms of products and the manufacturing process itself.


Where is Stäubli Robotics active?

Thanks to the precision and repeatability of our robots, Stäubli completely fulfills the requirements necessary to support the world of medical devices. Our global network of OEMs and system integrators covers all of the specific applications of the industry’s manufacturing processes.

While robots are often used for transferring devices from one station to another, Stäubli robots can also be used for high-value process applications such as polishing implants and machining prostheses. 


Customer Success Story

The Victor Robot Range from Qwadra: Advanced Technology for Orthotics and Prosthetics

Qwadra develops innovative solutions to enhance prosthetic and orthotic manufacturing. With its Victor robots, the company provides reliable and precise technology, enabling the design of orthotic and prosthetic (O&P) devices tailored to the specific needs of each patient.

 

Automated, precise, customized manufacturing

 

Victor robots are capable of machining a wide range of materials, including rigid and flexible foams, resins, technical polymers and wood, with high precision. Stäubli’s intuitive software optimizes 3D modeling, allowing precise adjustments and efficient tool path management. The result is a manufacturing process that supports the production of highly customized medical devices.

 

Flexible and customizable technology

 

Stäubli’s 6-axis robots, equipped with advanced options such as modular workstations with synchronized external axes, offer maximum customization, optimizing the solution’s efficiency. Application customization, diverse end effector options, automated tool changes and other features are designed to improve efficiency and reduce machining time, ensuring fast production of high-quality orthotics and prostheses.

 

Automation and customization: A solution to meet industry demands

 

The automation integrated into the Victor range optimizes production timelines while maintaining the necessary customization of each medical device. The robot settings adjust to product specifications, ensuring optimal comfort and precise physiological adaptation for patients.

With the Victor range, Qwadra provides device manufacturers with a flexible, high-performance technological solution designed to streamline O&P production. Manufacturers gain precision, speed, and reliability with technology engineered to support specialized production needs.

 

Watch the video to learn more


Personalized medical devices and robotics integration

Automation is particularly critical for high-value single-use devices, where precision assembly and rigorous testing are central to production. Surgical instruments such as staplers and pacemakers, which often comprise numerous components, require carefully controlled assembly processes to meet the highest quality standards.

The medical device industry is increasingly shifting toward customization, requiring highly adaptable manufacturing processes for products like invisible brace aligners and smart drug delivery systems. Robotic automation plays a crucial role. For example, to help manufacturers meet demand for invisible brace aligners, Stäubli robots are integrated into laser cutting applications. The ability to rapidly adjust cutting trajectories ensures precise customization, allowing manufacturers to accommodate individual patient needs. This customization process begins with an oral scan at the clinic, which generates a 3D model of the patient’s teeth. The model is then transferred to the factory, where robotic automation initiates production. Once completed, the finished aligner is delivered either to the hospital or directly to the patient, demonstrating how robotics streamlines personalized medical device manufacturing from digital design to final delivery.

Precise seam welding cell for helium tight implant welding under inert gas - CAM-guided, product flexible, fully automatic and MES-integrated. Image: Baumann GmbH


The future of robotics in medical device manufacturing

As medical device production evolves, manufacturers are increasingly leveraging data-driven automation to enhance traceability, efficiency, and compliance. Connected monitoring systems optimize performance by enabling real-time analytics, supporting industry-wide shifts toward predictive and adaptive workflows.

Stäubli Robotics provides you advanced automation solutions tailored for the medical device industry and broader life sciences sector. Our portfolio includes ESD-safe, cleanroom-compatible, and GMP- and FDA-compliant robots, designed for aseptic and harsh environments, ensuring manufacturers can meet regulatory requirements while maintaining operational efficiency. 


Medical Robotics

Pioneer in Medical Robotics

As a pioneer in medical robotics, we are working in close collaboration with highly specialized medical technology manufacturers around the world to develop innovative robotic solutions. Staubli Robots work hand in hand with health professionals as medical and surgical assistants in 4 areas: Surgery, Rehabilitation, Imagery, Diagnostics. For 30 years, Stäubli has been active in medical robotics, evolving around ISO 13485 standards to deliver a range of 6-axis robots that meet the market’s need for optimum precision, rigidity, patient safety and cleanability. We offer a wide range of options (Handguiding, Customization, etc.) to meet the needs of this market. We can also support our clients in their development by offering Co-Creation or Co-Development.

in line with international standards ISO 13485:2016


High Precision robots as medical and surgical assistants

What has long been standard practice in industry is now finding new applications in the field of medicine. Medical robots are on the advance, not only in the production of drugs, but also in medical applications. If you, as a medical equipment manufacturer, require high-precision, rigid and flexible robots that also meet all the criteria for medical environment conditions, we are your partner of choice.

Stäubli Robotics as your partner for proof of concept and research medical projects


MedXguiding Function

The innovative new MedXguiding function, coming soon to our TX2-60L MedX Ready robot, is set to transform medical procedures with an intuitive manual guidance option, becoming your reliable “second hand.”

 

The fully adaptable and configurable TX2-60L MedX Ready robot gives you the power to customize its functionality to meet your unique application needs. This flexibility boosts its usefulness across different medical settings, enhancing precision, effectiveness, and outcomes.

 

Designed with your needs in mind, the TX2-60L MedX Ready robot delivers exceptional precision for use in robot-assisted surgery and other medical applications. It is designed to address the specific demands of the healthcare sector, including orthopedics, surgical oncology, diagnostics, imaging, and rehabilitation. By focusing on precision, rigidity, patient safety, and cleanability, the TX2-60L MedX Ready is an ideal choice for enhancing medical interventions.

 

Our TX2-60L MedX Ready is ISO 13485 certified, ensuring strict adherence to industry standards. This certification reflects our commitment to delivering the high reliability and maximum safety that medical environments demand.

 

The new MedXguiding function promises to reduce tedious tasks, allowing you to focus on achieving excellence in patient care.

 

Watch the video for more information


Success Stories

Empowering surgeons, improving lives

Alaya, the first innovative robotic assistant for seamless spinal procedures

Founded in 2017, Cyber Surgery is a startup in San Sebastian, Spain that developed a robotic system for spinal procedures. The solution guides the surgeon to make the procedure safer, more accurate, and minimally invasive.

The main benefits are:

  • Reduced need for reintervention due to the robot’s accuracy
  • Shorter postoperative hospital stays with minimally invasive surgery

Explore the video


German Hospital ROSA® System

ROSA®: Robotic-Assisted High-Precision Implant Positioning

 

The knee joint is among the body’s most complex and key to mobility. Turning, rolling and gliding rely on the coordinated interaction of bones, muscles, ligaments and tendons, crucial to strength and function. Any change in this mechanism can cause conditions like gonarthrosis.

 

At Klinikum Hochrhein, a ROSA® surgical robot enables precise implant positioning, adapted to anatomy and optimized for soft tissue tension. Under ZOWU, the hospital has organized three orthopedic-surgical clinics in the Center for Orthopedics, Spine and Trauma Surgery. Surgeons report that ROSA® optimizes position and tension, ensuring the best adjustment and strong prospects for healing, function and durability.

The surgical robot ROSA® is in use at Klinikum Hochrhein for knee prosthesis surgeries.

Image: Klinikum Hochrhein


The Automation Boom in Diagnostics

Diagnostics is a distinct segment within the pharmaceutical sector. While other segments focus on manufacturing drugs or drug delivery systems and packaging, diagnostics are present in the lives of everyday people.

The advent of personalized medicine, which involves adapting treatments to individual patients’ characteristics and disease states, marks a significant leap forward in healthcare. However, this level of accuracy in medicine remains very expensive. In order to optimize therapeutic schemes and increase the effectiveness of treatments, diagnostic tests are essential. This predictive medicine makes it possible to anticipate clinical responses and adapt treatments for each patient.

Alongside these developments, the market is maturing and being shaped by the same trends affecting the pharmaceutical sector as a whole. The diagnostics segment was also impacted by the COVID-19 crisis, with entire populations taking multiple PCR tests during those years.

The automation of diagnostic tests is not new. Compact machines for applications such as automated plate handling, liquid handling, and storage and retrieval are widely installed in hospitals and healthcare facilities. The drivers are clear: cost reduction, more affordable treatment, the ability to treat more patients, and a lower risk of errors.

A flexible, robot-enabled benchtop cell

The main area for robotics remains benchtop cells, where operators place samples into a feeder, run tests automatically, and receive clear results within hours. These machines, often integrating Cartesian robots, grew out of drivers like the speed and precision of automation, safer solutions for reliable results, and long-term durability. These features align with the priorities of the machines’ manufacturers, but newer requirements demand enhancements such as compactness and flexibility. Single machines with Cartesian robots are designed only for a single test, but automation has evolved toward more flexible systems with compact footprints and advanced robotics.

Six-axis robots combined with tool changers easily perform multiple tasks in a single compact cell. For example, they can handle a PCR plate and then deftly transition to vial handling with only one pre-programmed sequence and tool change. These robots offer various reach options based on the tests being integrated, bringing an extended solution to the market.

To reduce the risk of contamination, the 6-axis robots are also available in versions designed for easy cleaning with various media, including resistance to aggressive H2O2 used for sterilizing isolators in drug production, increasing the quality of results.

Industrial and mobile robots already manage tasks like biobank management, pipetting, centrifuge loading, and PCR plate handling. The automation trend is booming in the diagnostics industry – not to replace operators, but to address labor shortages and meet growing demand. This shift also serves to relieve operators of repetitive tasks, reducing the risk of neuromuscular problems.