Food industry success story

Washing, foaming, rinsing

Benefits:

  • Reliable compliance with hygiene requirements
  • 500% faster processing
  • More even removal, less waste
  • Reduction of physically demanding work
Stäubli AG - Plangger20_Personen1_f_tim-2x-71610-jpg-orig.jpg
Plangger Junior Manager Reinhard Brunner (center) with Julian Bstieler of Dessl Maschinenbau (left) and Rudolf Staffler of Stäubli Tec-Systems (right).
Stäubli AG - Plangger20_bestreichen2_f2_tim-2x-71598-jpg-orig.jpg
Flexibility: Coating the smaller Sennkäse cheese with an herb-rock salt mixture takes place in 20-second cycles.
Stäubli AG - Plangger20_Fraesen11_f_tim-2x-71602-jpg-orig.jpg
In a cycle time of around two minutes, the rind is shaved off at a constant depth with exact path tracking. Previously, the strenuous manual scraping process took around 10 minutes per block.
Stäubli AG - Plangger20_reinigen3_f_tim-2x-01-71614-jpg-orig.jpg
The robot is internally pressurized up to 50 mbar so that no cleaning agent can penetrate from the outside. It withstands high-pressure hot water jets, foaming with chemical detergents, and manual brushing.

TASK

Automated de-rinding of cheese

At an organic cheese dairy in the Austrian Tyrol, a Stäubli six-axis robot is busy de-rinding and coating irregularly shaped blocks of cheese, a demanding job that calls for maximum resilience. The TX2-90 HE is able to withstand intensive cleaning with aggressive detergents delivered by a high-pressure lance – a treatment that would soon spell the end for the average standard robot.

At any one time, up to 650 tons of organic cheese made with milk from the finest Tyrolean hay-fed cows are maturing in the 160-meter-long, 10-meter-high man-made cave of the Plangger cheese dairy in Niederndorf (Tyrol). Since early March 2020, a series of otherwise strenuous tasks have been carried out in a fully automated robot cell. A ceiling-mounted Stäubli TX2-90 HE (humid environment) handle the entire de-rinding of cheeses as well as the coating of Sennkäse cheeses.

In the past, the hard rind was removed manually with a scraping iron. This took about 10 minutes per 600-millimeter block and required immense physical effort on the part of the employee. Today, the robot does the job more accurately and economically than ever before.

 

SOLUTION

Fast and precise de-rinding performed by a robot

The Stäubli six-axis robot shaves the rind off the unevenly shaped cheese rounds with high accuracy thanks to 3D path tracking. Further, with a cycle time of around two minutes per cheese, the TX2-90 HE is approximately five times faster than a human doing the same job. Coating the smaller Sennkäse cheeses is even faster, with a cycle time of 20 seconds, which is equivalent to 600 kilograms per hour.

The first step of the process involves paring the top and perimeter. The cheese is automatically lifted from the belt by a vacuum suction gripper and placed on a rotary table. The robot does not begin its work until the cheese has been measured by laser, since the blocks are irregular in shape and no two are ever identical. The paring tool can then begin to remove the rind, with the Stäubli control system adjusting the distance between the blade and the surface in real time.

When the time comes for the underside to be de-rinded, the handling unit grips the cheese at the center, swivels it around, and places it on a second rotary table. Here it is measured by laser again before the final stage of de-rinding proceeds. When this a completed, the block is lifted and placed on the discharge conveyor belt.

 

CUSTOMER USAGE

Top-level output, quality and hygiene

The already stringent specifications that apply in the food sector are taken to an even higher level in cheese manufacture, due to the deliberate use of bacteria. Cleaning of the Plangger plant is therefore carried out with fat-dissolving, alkaline and milk stone-dissolving acidic agents as well as with water at 55°C. The robot cell is robust enough to withstand cleaning procedures with a high-pressure lance which are necessary several times a week.

The Stäubli six-axis HE robots are conform to HACCP and have a unique hygiene concept. There is no other truly viable alternative to using these robots in combination with H1 oil, which is the only kind approved for direct food contact. They have a particu