USA based Arcadia Aerospace Industries provides the aerospace sector with state-of-the-art inspection solutions. The company has developed advanced instrumentation and automated systems that make a valuable contribution within the carbon fiber composite laminate, and structural component markets.
When tasked with developing a robot based non-destructive testing system, which would require around 100 DC electrical connections, 8 data connections, 3 high flow valved fluid connections, and high-powered AC electrical connections, Arcadia Aerospace clearly had multiple challenges to overcome:
Overcoming these challenges would require the use of an automatic robot tool changer, however any unit chosen would have to be capable of integrating multiple modules to provide the complex connectivity required.
The Only Turnkey Solution on the Market
Recognized worldwide as a leading technological pioneer in the design and development of robotic tool changing systems, Stäubli was approached by Arcadia Aerospace to assist in the configuration of an automated tool changing system. This solution would need to integrate seamlessly with their TX200 robots and also address the complex requirements of this application.
The solution to this demanding application is based upon Stäubli’s customized option, which allows the configuration and construction of special, application-specific solutions:
The result of Stäubli’s collaboration on this project is a customized turnkey solution from a single supplier, which not only meets all the application requirements but has the flexibility to allow it to be utilized across many different testing procedures, including but not limited to conventional UT, laser scanning, and flash thermography.
Almost a 100% Decrease in Tool Change Time
The ability to have several technologies in one compact package has resulted in a smaller tool changer footprint while completing testing.
In addition to saving space, using the automated tool changer has exponentially increased throughput on the robot cell. Before integrating the automated tool changer on the systems, customers needed to undertake a time-consuming manual process, switching between the various testing technologies. Whereas the manual changeover process took anywhere between 30-60 minutes, the same changeover, using the automated tool changer, takes only 30-60 seconds to complete. The synergy between Stäubli Fluid Connectors, Stäubli Robotics, and Stäubli Electrical Connectors has delivered tremendous value for Arcadia Aerospace:
Arcadia Aerospace Industries was founded in 2008 with a mission to provide the aerospace industry with state-of-the-art inspection solutions by effectively utilizing the philosophies of high quality, advanced techniques, and superior customer service. AAI’s leading aerospace composite inspection technology team utilizes proprietary technology and extensive aerospace expertise to provide aerospace and industry leaders with cost-effective, time-efficient and superb-quality solutions to advanced metal and composite material challenges in inspection, engineering, quality and special process manufacturing.
Mark Pope