Stäubli has been working in partnership with the aerospace industry on major international projects for over 40 years. It is recognized for its expertise and ability to supply connection solutions which perfectly meet the specific requirements of these critical sectors. We specialize in delivering the exceptional safety, light weight, compactness and cleanliness these industries demand for a range of applications such as air conditioning, breathing air, compressed air, fuel, hydraulics and thermal management.
Quick-release couplings on air-conditioning components (compressor, condenser, evaporator), enable assembly and disassembly of the system without draining and refilling the refrigerant circuit.
In the commissioning phase or for deeper maintenance processes, the line must be completely drained and refilled. Stäubli connectors facilitate this process quickly and reliably.
Stäubli high-flow, flat-face couplings deliver maximum reliability, while pressure-relief systems ensure safety.
Electronic components are increasingly cooled by liquid-filled cold plates. Bayonet locking systems provides a high degree of ergonomic and safety.
For compactness reasons cold plates must be racked in a chassis. CGO and CGD couplings allow connection without spillage and level out different misalignments.
From the refinery to the consumer, fuel logistic requires many connection points. Whether STANAG or specific dedicated profiles, Stäubli assures safe and non-spill connections.
Quick connections are the key to completing testing processes in the best conditions of safety and quality.
Airport processes demand flexibility. Quick-release couplings from Stäubli deliver optimum efficiency in modular systems.
Extrem temperatures and humidity conditions require the aircrafts to be preapared with a spray of glycol on their surface. Glycol logistic can be simplified with the use of quick release couplings.
Fuel connection from tank to engine and everything in between. Coolant and heating lines: Quick, secure and non-spill connections from engine to radiator and heating system.
For braking and steering. High or low pressure, vibrations, shocks and/or pressure picks, Stäubli connectors are compliant to those difficult environments.
Stäubli test-bench connectors eliminate the risk of misconnection, improve quality, and reduce process-preparation time.
In the commissioning phase or for deeper maintenance processes, the line must be completely drained and refilled. Stäubli connectors facilitate this process quickly and reliably.
Quick change of the radiater for replacement or access to other parts of the engine. Connection to the heater inside the cabin, all without purging the line.
Quick-release couplings on air-conditioning components (compressor, condenser, evaporator), enable assembly and disassembly of the system without draining and refilling the refrigerant circuit.
The oxygen supply at different locations of an hospital must be deployed rapidely but with caution, the connection must avoid pollution in the line. Flat face coupling technology complies with this requirement.
Stäubli connectors ensure high-pressure bottles are connected safely during filling and use.
Emergency situations or harsh environments require human operation and an autonomous breathing air system must be used.
High pressure filling is a delicate operation due to the adiabatic pressure. A specifc coupling must be used for the quick connection of the bottles to the high pressure supply line.
In the fuel cell and further in the batteries, heat is generated and must be evacuated. Liquid cooling lines are embedded and so the requested time for the maintenance process can be reduced with appropriate QRCs.
High pressure hydrogen bottles can be rapidely connected to the supply line. After the filling process, the pressure is released for disconnection
After expansion, the low pressure hydrogen is led to the fuel cell. The maintenance of the sytem is simplified by the connection with QRCs.
From the high pressure bottle to the pressure reducer, the line can be connected and disconneted with the dedicated coupling