HEALTHCARE - LIFE SCIENCES Patient Care

High-precision robots as medical and surgical assistants

Helpful hands redefined: What has long been standard practice in industry is now finding new applications in the field of medicine. Medical robots are on the advance, not only in the production of drugs but also in the operating theater. If you, as a medical equipment manufacturer, require high-precision, quiet and flexible robots that also meet all the criteria for sterile surgical conditions, look no further than the Stäubli range. Easy to clean, with minimal particle emissions and high precision, they relieve doctors of some of the strain they are under while performing operations that demand their full concentration. Robots are also contributing to the development of innovative surgical techniques.

Success stories - Applications
Stäubli AG - cancer-surgery-robot-pim-2x-68222-jpg-orig.jpg
Cancer treatment of the future (SEON)

Chemotherapeutic measures are an immense burden for cancer patients, as the high-dose drugs that circulate through the body to fight cancer cells also affect healthy cells. The SEON research project at University Hospital Erlangen aims to use a robot to precisely combat solid tumors or metastases.

Stäubli AG - BHSTechnologies-AT-pim-2x-65815-jpg-orig.jpg
RoboticScope brings dynamic improvements to the operating theater (BHS Technologies)

Ocular lenses and microscopes are reaching their limits in microsurgery. A start up company has invented a unique robot-assisted camera system that gives surgeons completely new insight into the operating field via a head-mounted display.