Exploring the future in textiles – TF 20 weaving system

The study of new material mixes, mainly carbon and/or ceramics, and new applications specifically for various industries – that's the purpose of the TF20 weaving system recently installed at the Hof University of Applied Sciences in Germany (more precisely, the Institute for Material Sciences). Here, renowned researchers and their students pursue their daily quest for new materials, studying their behaviour in various production processes, including weaving. The institute works with the renowned Fraunhofer Institute, which allows an opportunity to conduct research on ceramic fibre production and processing.

Demanding applications and materials

To fulfil the forward-looking weaving ambitions of the institute, researchers and students, their shedding solution must allow unlimited binding possibilities and the weft insertion system must feature a double rapier. The materials being processed are mainly carbon and ceramics. Carbon is used in lightweight solutions for aircraft fuselages or automobile bodies, and ceramics are used where heat resistance is essential, e.g. in ceramic parts for aircraft turbines. Highly heat resistant, ceramic parts do not require steady cooling down, which lowers overall energy consumption.

Both materials have properties that require specially constructed weaving machinery. Carbon is conductive, so it requires encapsulated electronics and liquid cooling to avoid short circuits. Ceramic fibres are very brittle, so these yarns require extremely gentle handling, especially during shedding.

Customer benefits

The staff and students benefit from having state-of-the-art technology at hand for research and projects in their new competence center.

Solution

To meet above mentioned challenge, Stäubli developed a special carbon version of the TF20 technical weaving system. It includes an encapsulated UNIVAL 100 Jacquard machine. Furthermore the system solution is enhanced with valuable Stäubli support regarding binding techniques.

Product solution for this type of application

Stäubli success stories