Automotive Success story

Parts inspection with a twist

Customer benefits:
  • In-line X-ray inspection for zero-defect production
  • Highly flexible system technology
  • Seamless documentation and traceability
  • Effective alternative for managing a shortage of skilled workers
Stäubli AG - Kiekert20-CZ-1-tim-2x-68094-jpg-orig.jpg
The gripper seals the opening to the X-ray chamber during inspection, which requires the part to be rotated 180 degrees.
Stäubli AG - Kiekert20-CZ-2-tim-2x-68095-jpg-orig.jpg
The inspection system has a compact footprint.
Stäubli AG - Kiekert20-CZ-3-tim-2x-01-68101-jpg-orig.jpg
Inside the compact cell are a robot, a camera, and an X-ray chamber.
Stäubli AG - Kiekert20-CZ-4-tim-2x-68106-jpg-orig.jpg
The X-ray inspection is thoroughly visualized and documented.

TASK

Robot-assisted X-ray inspection of vehicle locking systems

Kiekert is the world’s biggest manufacturer of automotive locking systems. At its largest plant in Prelouc, Czech Republic, a workforce of some 2,400 produces around 180,000 side door latches a day on 60 assembly lines.

Among the numerous automated assembly and testing tasks involved is the 100% inspection of soldered connections. A high-precision Stäubli robot has the job of manipulating the latches as they pass through a compact X-ray inspection cell.

The latest development in the design of these locking systems is the incorporation of convenience functions such as Kiekert’s proprietary Kiekert “Soft-Close” mechanism. As with all motor vehicle locks, the zero-defect principle applies. Consequently, the production engineers at Prelouc sought a way to subject the soldered connections in the plastic casing to 100% inspection.

 

SOLUTION

In-line X-ray inspection of soldered connections

On detailed analysis, it was determined that X-ray inspection would be the best technology for 100% inspection. A Czech company designed and built an inspection cell in which all handling tasks are performed by a compact Stäubli TX60 six-axis robot.

These include handling the test component during the inspection process in the X-ray chamber. The robotic gripper is designed to seal off the entry port to the chamber, thus preventing radiation leakage during the test. After the first X-ray image is recorded, the gripper rotates the latch 180 degrees and a second image is taken. Kiekert also wanted the capability to rotate the components in 5 and 10 degree increments – a requirement easily met by the high-precision TX60.

 

CUSTOMER USAGE

The self-learning test cell

The compact inspection cell includes a screen that clearly and unambiguously displays the test results, including the X-ray images. All measured values are documented and recorded for traceability. The testing process also has autonomous learning capabilities. If a soldering parameter is changed, for example, the test cell’s control unit can determine whether the change has had positive effects, based on the number of usable and defective parts.

Yet another beneficial feature of the robotic test cell is its flexibility. The sy