September 16-21, 2019, Hannover

Advanced robotics solutions for the metalworking industry

The TX2 six-axis robots and the TS2 SCARAs are reliable, fast and accurate even under the most challenging conditions.
The phenomenal amounts of cooling oil have no adverse effect on the fully encapsulated TX40.
The Stäubli six-axis robot can easily withstand the conditions inside the grinding machine.

At EMO Hannover, the world's leading trade fair for machine tools and metalworking, Stäubli will be presenting a bespoke full-range program for applications in the industry. Our globally unique portfolio includes the new completely encapsulated four-axis and six-axis robots of the TS2 and TX2 generation which are able to withstand direct contact with grinding dust, metal swarf and cooling lubricants.

Visit us on our booth B42, Hall 9 to see the quality performance of these machines. Watch one of the compact six-axis TX2 60L working away inside a machine tool cell and performing reliably under the toughest conditions.

Another standout feature at the trade fair will be our mobile robot system HelMo, which can handle the loading and unloading of machine tools as well as linking them into a single assembly line. We will also be demonstrating the type of tasks that can be performed by our Power Cobot TX2touch in direct collaboration with human employees.

Get an idea of the productivity gains that can be made with our robots and software products in the area of Industry 4.0 and digital networking. We are confident that you will be impressed by the superior performance of these products, which will be on show at our stand (B42 in Hall 9). The Stäubli exhibition team looks forward to meeting you in Hannover.