HEALTHCARE - LIFE SCIENCES MEDICAL RESEARCH & DEVELOPMENT

Research & development: robots soon to be indispensable

Deadlines and precision are crucial in R&D in every aspect, be it automated cultivation of cells or robot-assisted sample handling. If you are a research institute or company looking for automation solutions, you have come to the right place. If, for example, your business involves the preparation of cells for high flow rate measurement methods or the filling of culture media, we can help.

If you still handle complex tasks manually, Stäubli can deliver the perfect solution for automating them. Of course, as a company with a long tradition of innovation, we also excel in pioneering applications such as robot-assisted oncological treatment.

Applications
Stäubli AG - GRC2021_IMG_8050f_pim-2x-77383-jpg-orig.jpg
Stäubli six-axis machines in pharmaceutical research (GRC)

The Genomics Research Center in Taipei employs a now well-established ultra-high-throughput screening (uHTS) system to identify active substances that are effective against COVID-19. A highly dynamic Stäubli six-axis RX160 is at the heart of the system.

Testing treatments for childhood diseases with a RX160

Testing treatments for childhood diseases

Researchers use Stäubli robots to test potential treatments in experimental projects. The result: in one week, the RX160 6-axis robots conduct millions of experiments faster and more accurately than any human could.

Systems for a wide range of tasks with a TX40 cleanroom

Systems for a wide range of tasks

The field of scientific research benefits from innovative robotics solutions. Stäubli’s line of compact TX Cleanroom robots gives researchers access to exceptionally state-of-the-art automation solutions.