March 1, 2021


STÄUBLI | BREAK-AWAY

A complete range of high-performance safety break-away couplings

Stäubli now has a complete range of high-performance safety break-away couplings designed to prevent tear-related accidents that can occur on different types of industrial applications. This new line of large bore couplings, which are used on high-flow applications, broadens the range of anti-pollution couplings. 
Stäubli continues to place the safety of people and equipment at the heart of its work. 
This only strengthens its position among the leaders in innovative connection solutions for fluid logistics.

Solutions to prevent accidents
Under certain operating conditions, equipment can be subject to excessive tensile loads, particularly in the event of a malfunction or incorrect handling. This includes times when hoses used at sea are subject to extreme lateral forces, or during truck or rail tanker loading and unloading operations.
Stäubli's safety break-away couplings enable the mobile unit to disconnect from the loading system above a defined tensile load, without breaking or spilling any fluid.
These high-performance solutions respond specifically to the requirements of each application that require fluids to be transferred safely: chemicals sector, rail, marine, offshore, oil & gas, LNG, etc...

The safety of people and installations is our priority
Whether positioned between a fixed point and a hose line, or between two hoses, Stäubli's safety break-away couplings ensure the safety of operators, prevent fluids from polluting the environment, and protect your installations.
Safety is guaranteed by the immediate disconnection of the coupling, which is triggered by a separating mechanism (breaking pin or cable), and the automatic closure of the flow line.

Each application has a Stäubli solution
Stäubli has developed appropriate solutions for more specific applications, such as uses in marine or offshore environments. This includes connections between two hoses that must withstand extreme lateral forces.

Stäubli products are designed to protect people's safety, ensure the durability of equipment, protect the environment, and contribute to the productivity of companies.