Agenda

What are the topics? 

Agenda

Stäubli Pharma Focus – Partner Innovation Day 2024

 Timeslots  CompaniesTopicsSpeakers
8.30-9.00 Arrival and Registration / Coffee 
9.00-9.05Stäubli RoboticsWelcome SpeechRudolf M. Weiss
9.05-9.45  Rychiger AGSmall batch production in Pharma production and its implications on operations and machine designJames MacKenzie & Alessio Maiocchi
9.45-10.00Stäubli ECSSafe and durable connections for the Lifescience industryAlain Angly
10.00-10.45 Networking & Coffee Break 
10.45-11.15Stäubli RoboticsSterimove – Modular, Collaborative & Easy-to-Clean mobile pharma robotFernando Cazzato
11.15-11.45Wilco AGEngineering challenges for high-mix/low-volume visual inspection solutionsAlex Schäfer
11.45-13.30 Business Lunch & Visit of Exhibition 
13.30-14.00Pharmabotix AGModular and Flexible Robotic Solutions for CGT and Lab: User-Friendly, Future-Oriented, and EfficientFabian Stutz
14.00-14.30SKAN AGRobots for small batch production of sterile pharmaceuticalsMax Mittelviefhaus
14.30-15.15 Networking & Coffee Break 
15.15-15.45Watson Marlow AGRequirements for single-use systemsMarco Renggli
15.45-16.15Stäubli FCSCoupling solutions for the pharmaceutical and cosmetics industriesOliver Beckmann
16.15-16.25 Closing Q&A and "Farewell" 

Presentation Topics

Rychiger AG

9.05 - 9.45 h

Topic

Small batch production in Pharma production and its implications on operations and machine design

The rise of personalized medicine and increasingly complex, unpredictable forecasts have led to significant disruptions in the supply of medicines. These challenges are primarily due to the inflexibility of current manufacturing lines used in the pharmaceutical industry. This presentation explores potential solutions to these issues, focusing on how the challenges presented by small and micro-batch production can be overcome.

Speakers

James MacKenzie

Sales Director at Rychiger Pharmatech AG

Alessio Maiocchi

Product Manager LifeScience and Digitalisation at Rychiger AG

Stäubli ECS

9.45 - 10.00 h

Topic

Safe and durable connections for the Lifescience industry

In the healthcare and medical markets, the absolute reliability of all components is extremely important. Electrical, hybrid and modular connectors are no exception: their constant availability and fail-safe operation are essential. Let’s learn more about these features in a case study.

Speaker

Alain Angly

Sales Manager at Stäubli ECS, Switzerland

Stäubli Robotics

10.45 - 11.15 h

Topic

Sterimove – Modular, Collaborative & Easy-to-Clean mobile pharma robot

In order to fulfil the strict regulatory requirements of EUGMP Annex 1, the pharmaceutical and biotechnology industries often calls for a compact mobile robot platform. Designed for sterile applications, the Sterimove seamlessly integrates processes such as environmental monitoring, loading freeze dryers, performing quality control processes and more. It ensures that sterility is maintained in cleanrooms and sensitive production areas to produce sterile products. Discover with us the possibilities offered by this unique platform to fulfil regulatory standards, increase efficiency, and maintain the highest levels of cleanliness.

Speaker

Fernando Cazzato

Local Head of Pharma Robotics at Stäubli Robotics, Switzerland

Wilco AG

11.15 - 11.45 h

Topic

Engineering challenges for high-mix/low-volume visual inspection solutions

With the arrival of Advanced Therapy Medicinal Products (ATMPs) as well as a rise in personalized healthcare, there is an increasing demand for visual inspection solutions for products with low to very low volume and high product variation. The production of high-mix/low-volume medicines pose challenges for fully automated visual inspection (AVI) systems that are geared towards high throughput. Is there way to combine the output, process safety and reproducibility of an AVI system with the flexibility and short lead time of a manual visual inspection (MVI)? This presentation gives an insight into the various challenges that pharmaceutical and equipment manufacturers and the interest group for visual inspection at large face and how they can be addressed.

Speaker

Alex Schäfer

Technical Product Manager at Wilco AG

Pharmabotix AG

13.30 - 14.00 h

Topic

Modular and Flexible Robotic Solutions for CGT and Lab: User-Friendly, Future-Oriented and Efficient

Maximum flexibility in the fields of Cell and Gene Therapy (CGT) and laboratory environments is key to the success. But how can this be effectively achieved? How can various containers, consumables and processes be integrated into one solution? The answer lies in a user-friendly HMI, smart engineering and advanced, flexible robotics. Using an example of inoculum production, the presentation will demonstrate how different containers, pipettes, and lab devices can be efficiently combined into a compact and flexible system.

Speaker

Fabian Stutz

CEO & Owner of Pharmabotix AG

SKAN AG

14.00 - 14.30 h

Topic

Robots for small batch production of sterile pharmaceuticals

Robotics are finding more and more application in the manufacture of pharmaceuticals, for example in small batch production. The necessary flexibility inherent to production of small batches requires appropriate solutions and is further potentiated by the demands that need to be met for filling of sterile products.

As worldwide leading manufacturer of isolator systems for aseptic drug manufacturing, SKAN will discuss about the requirements for robots in aseptic environments. The presentation is centered around a case study highlighting the collaboration between Stäubli and SKAN to drive the development of new features for the Stericlean package to ensure that Stericlean+ robots are suitable for integration into pharmaceutical isolators and operation under aseptic manufacturing conditions. Key presented developments include appropriate material selection, design of robot surfaces for efficient cleaning and decontamination, as well as characterization of particle generation from moving parts.

Speaker

Max Mittelviefhaus

Head of Research  and SKANalytix at  SKAN AG

Watson Marlow AG

15.15 - 15.45 h

Topic

Requirements for single-use systems

Single-use systems have become established in biotechnology and are also increasingly being used in the sterile production of pharmaceuticals. A key reason for this is that the costs for cleaning are significantly reduced compared to a stainless-steel system. In addition, cleaning validation is not required. Furthermore, the time to market can be shortened by eliminating construction work and faster scale-up. We will show you the various aspects of using single-use systems. Our experts from the field are available to answer your questions - come to the presentation with your questions.

Speaker

Marco Renggli   

Life Science Sales Engineer at Watson Marlow AG

Stäubli FCS

15.45 - 16.15 h

Topic

Coupling solutions for the pharmaceutical and cosmetics industries

Stäubli develops fluid-line coupling solutions in response to the challenges facing the fine chemicals sectors, pharmaceutical laboratories, biotechnology, and the cosmetics industry. Sterilizable quick-release couplings without retention areas maintain product integrity and are made using materials suitable for corrosive atmospheres.

Stäubli connectors also ensure the safety of installations and operators. Mechanically interlocking, ergonomic couplings offer solutions for a wide range of applications, such as inserting of tanks and the provision of breathing air.

Speaker

Oliver Beckmann

Sales Responsible at Stäubli FCS, Switzerland